May 2024 Newsletter
CommScope Technical Family Webinar |
Join us for the next CommScope Technical Family webinar, “MPO Testing in the Data Center” on June 13th.
From the time data centers began deploying speeds of 40G/100G, there has been a transition towards parallel optics, which is driving the need for multi-fiber connector interfaces. Today we are seeing cloud scale data centers, AI clusters using InfiniBand, and ethernet networks where speeds from server rack-to-leaf and leaf-to-spine are using 400G/800G connections. These connections are using MPO based connectors which are available in 8, 12, 16 and 24 fiber MPO type configurations.
Due to non-blocking architectures, we see data center clusters using a high density of MPO connections. Typically, thousands of MPO connectors are required. Traditional single fiber testing method is labor intensive, time consuming and measures the individual fiber loss.
With higher speeds the loss budgets are shrinking, and this is putting additional focus on the connector and most importantly the overall channel link performance.
In this webinar, we will address MPO testing challenges and share some of use case scenarios and various methods used.
Register for this webinar here.

Solutions and Product Updates |
 The GigaREACH™ XL solution is the latest innovation in the SYSTIMAX® portfolio. GigaREACH XL supports 10Mbps Ethernet and 90W PoE up to 250 meters, 100Mbps Ethernet and 90W PoE up to 200 meters, and 1Gbps Ethernet and 90W PoE up to 150 meters (50% longer than Cat 6). These distances are available with SYSTIMAX Category 6 connectivity.
Box Style Package Option for Cat6A Small OD Cables
The “Reel-Less” box package, for our Category 6A small OD cable, offers installers and customers ease of set-up and transport. The “Reel-Less” box package easily breaks down flat for disposal, uses less space, has less waste and is recyclable.
- Proven and reliable box packaging technology for faster, efficient, and reliable tangle-free installations
- Easy to carry, stack and store
- Savings in time and labor

New Termination Tool
This new tool, JTT-HGS, will include an adapter to be used for the termination of the HGS620 jack. This enhanced termination tool incorporates features such as a cable stripper and a shield scoring tool. Repetitive quality of crimping is assured when applying the new tool in combination with the adapter.
Ordering Information:

Customers who are currently using the termination tool 1725150-3 or 1725150-6 with revision J or higher will be able to use this separate adapter as well and can order a pack of five pieces. (MID 760257785).
Key Features
- Terminates the HGS620 jacks
- All in one termination tool
- Strips cable, marks foil and terminates eight conductors at once
Click here to watch the HGS620 Jack Termination video.

CommScope offers products to bond interlocking armored fiber. If you search BLK-ARMOR on commscope.com, you will see a complete list.
Follow the CommScope Enterprise LinkedIn page to be in the know on latest news and updates on fiber and copper structured cabling solutions. Be future-ready and expand the performance and application potential for buildings, data centers and campuses.

Check out this recent episode of the CommScope Crosstalk podcast: “Powering the Future – A Conversation with Stephen Eaves, the Inventor of Fault Managed Power.”
Click here to access. You can listen on your mobile device through Spotify, Apple podcasts, and all other major podcast streaming platforms.

CommScope's Technical Assistance Center (TAC) |

Welcome to SYSTIMAX® 2.0

Regional TAC agents are ready to provide you 24/7 on-line technical assistance.
That is the SYSTIMAX 2.0 Assurance!
Contact us: https://www.commscope.com/support/enterprise-networks/
Always…Start with the TAC!
We make it easy:
Where are you located? Email a TAC agent in your region (24x7) and get a quick reply:
North America: tac.americas@commscope.com
Europe, Middle East and Africa: tac.emea@commscope.com
Central America, Latin-America, Caribbean: tac.cala@commscope.com
Asia-Pacific: tac.apac@commscope.com
Prefer to Chat?
Start a live chat with a TAC agent in one click: LiveChat. 24 hrs. Mon-Fri
We would like to hear from you! Please share your feedback and suggestions on the CTF newsletter here.
|